Part Number: LM74701-Q1 Tool/software: Hi,
the datasheet states:
(8.3.4) ... The EN pin can withstand a voltage as large as 65 V and as low as –33 V. This feature allows for the EN pin to be connected directly to the ANODE pin if enable functionality…
Part Number: AM62A7-Q1 Other Parts Discussed in Thread: AM62A7 Tool/software: HI, TI
Now,We develop AM62A7 on ti-processor-sdk-linux-edgeai-am62axx-evm-09_02_00_05
We get rootfs by compiling yocto-build.
We have a confusion that the system time…
Part Number: AM62A7-Q1 Other Parts Discussed in Thread: AM62A7 , AM62A3 Tool/software: Hey there,
I have two questions regarding the power supply and the design of the eval board (AM62A7 / AM62A3 LOW POWER STARTER KIT SK (EVM) WITH TPS65931211-Q1 PMIC)…
Part Number: DLPC120-Q1 Tool/software: Hi,During the test of our DLPC120+DLP3030 system, RE did not meet the requirements (AV value of about 76MHz exceeded 3dB). After investigation, it was caused by the clock at the DMD interface. We have done shielding…
Part Number: Tool/software: WEBENCH® Design Tools Hi,
There is some error in resolver to digital Tida00796 schematic. In the below diagram ,there are some red double cross sign in front of IE1,IE2,IZ1,IZ3,IZ2,IZ4.What is the meaning of those red crosses…
haitang wang said: we add the user muticast address but not show on the ALE table,you can try add the new muticast address 。Thx
Hi Haitang
verified on SDK9.1 Jacinto7,
multicast frame can be received on A72 Linux
see following debug log:
-------…
Part Number: LM5069 Other Parts Discussed in Thread: CSD19532KTT
Tool/software:
Abstract
It was noticed that bad connection on the power supply cable can cause some sort of ‘fault loop’ on the LM5069 circuit, from which it usually cannot automatically…
Part Number: TL2575HV-05-Q1 I want to know efficiency calculation for this part number TL2575HV-05-Q1 with formula.
Vin = 54v and Iload = 500mA
Please reply me as soon as possibile.
Part Number: TMS570LC4357 Tool/software: Hello ,
Q1 -) i coundt find any document that shows the clock source of the ECAP module on the TMS570LC4357 mcu ? It shown as SYSCLK in the trm Figure 33-6. Counter and Synchronization Block , but what is SYSCLK…