Part Number: UCC28C42-Q1 Other Parts Discussed in Thread: LMV431 , TL431 , UCC28C42 Hi Team,
We would like to ask your help regarding the customer's inquiry below.
When I design the UCC28C42QDRQ1 with Webench the adjustable precision shunt regulator…
Part Number: TL431-Q1 Hi team,
I got a question from customer if there is a specification about the strain tolerance of package.
Customer need the strain tolerance of below device.
Product : TL431AQDBZRQ1 (SOT-23)
If there is such a specification, could…
Part Number: LM5156-Q1 Other Parts Discussed in Thread: TL431 , PMP10666 , LM5156 Tool/software: Dear TI Support Team,
I’m designing a flyback converter that outputs ±150V +-60mA, and while the overall circuit functions well in simulations, I’m having trouble…
Part Number: TL431-Q1 Other Parts Discussed in Thread: TL431 The used device is getting heat-up. Please the used ckt as attached.
Input voltage Typ = 24V +/- 4V
Output voltage Vz= 6.8V
Current flowing through TL431 is approx 25 mA.
Please look into the…
Part Number: TL431-Q1 Dear team,
My customer needs to compute FIT of TL431-Q1(A version), so they need to know the total transistor numbers of TL431-Q1. There is the detailed schematic as below, there are 11 transistors in the schematic. So TL431-Q1 has…
Part Number: UCC14241-Q1 Other Parts Discussed in Thread: UCC21756-Q1 , TL431 , UCC33420 Tool/software: Hi,
I am using UCC21756-Q1 gate driver IC for driving an SiC MOSFET. The power supply used to generate +15V and -5V for the gate driver is UCC14241…
Part Number: TL431-Q1 Other Parts Discussed in Thread: TL431LI-Q1 , TL431 Hello Folks,
I have a question about the stability boundary conditions. I my design i have VKA from around 5.1 V and Ika of 4.2 mA.
In the datasheet Figure 16, recommends that for…
Part Number: LM5156-Q1 Other Parts Discussed in Thread: LM5156 , UCC28600 , TL431 Tool/software:
Hi Team,
Do you have LM5156-Q1 DCM calculation tool to calculate compensation values supporting multi-outputs ?
LM5156-Q1 DCM desgin tool was discussed…
Part Number: TL431-Q1 Other Parts Discussed in Thread: TL431LI-Q1 , , TL431 Hi Team,
I am a bit confused by the minimum cathode current spec in the datasheet. Under recommended operation conditions, the minimum is specified at 1mA. However, the Imin spec…