Part Number: TL1454A Other Parts Discussed in Thread: TL5001 , TL1451 , TL1451A The thermal rating for the TL1454A appears to be -20°C to +85°C as shown in the absolute maximum ratings. I am curious what parameters or degradation happen if the device is…
Other Parts Discussed in Thread: TL5001 Hi team,
Could you let me know TI alternative for NJM2382?
EE: PAC indoor unit
Customer is using NJM2382 ac 1ch as 1ch opamp.
Thus i'd like to replace this opamp.
Best regards,
Kento
Hello,
Maybe TL5001 is an old part, but this part is a DIP package and can run up to Vin=40V... I will try to reduce output capacitor.
Best regards,
JB
Hi Jasper,
Some news. I have received my new PCB and I have done some tests with a load that consumes 8A.
TL5001 now runs as expected (@ 300 kHz). @300 kHz, efficiency is not very good (between 60 and 65%). @100 kHz, I have measured 80%. If I reduce frequency…
Part Number: TL5001A Other Parts Discussed in Thread: TL5001 Good evening,
I use for a long time TI controller to make DC conversion. On my last PCB, I use a TL5001A but I think I have done a mistake somewhere as this controller starts if and only if…
Other Parts Discussed in Thread: TPS2819 , TPS2818 , TPS2816 , TPS2817 , TL5001 , TPS2819-EP , TPS2818-EP Hello,
I was going through the datasheet of TPS28XX - EP. There was one Contradictory statement.
Statement in page 2 mentions -
"The TPS2816 and TPS2817…