Part Number: TL971 Other Parts Discussed in Thread: TLV9161 Accoording to the datasheet page 1 a SOT-23 package is available for the TL-971. However in the ordering part number table I do not find the orderingnumber for the TL971 in SOT-23 package.
…
Part Number: TL971 Other Parts Discussed in Thread: TL974 , , TL972 Hello,
there are several issues with the TL971 / TL972 / TL974 datasheet that need to be reviewed. To name some of them, without claim for completeness:
- The ESD ratings and some…
Part Number: TL971 Other Parts Discussed in Thread: ALP , DS90UB971-Q1 971 EVMs are not being detected over USB. I have tried this with 2 971 EVMs. If we connect the 971 EVM via aardvark, we are able to detect it. Please see the snapshot below of the…
Part Number: TL971 Hi team,
Good day.
Can you please confirm if the TL971 provides a bidirectional output current? Can it output a negative current? Regards, Carlo
Part Number: TL971 Dear;
When the TL971 doesn't connect TPS76301, the output of TL971 is normal, but when it connected to the input of TPS76301, the output of TL971 is decreased to 1V and its waveform is distortion. Could you please give me some advice…
Hi Ron, I still do not understand that you said. Q1: For figure 1 and figure 2, they are differences are φM and f0. But what are the φM and f0? Q2: For figure 1 and figure 2, you mean that find gain 0dB, go vertical to phase line, then the intersection…
Part Number: TL971 Other Parts Discussed in Thread: TINA-TI I have a TL971 in a simple voltage follower configuration. I plan on using the TL971 to buffer an audio signal for greater amplification.
When the input signal nears the rails, the output…
Other Parts Discussed in Thread: TL971 Hello Sir
Please suggest the application ckt of TL971, which we want to use as audio preamplifier to amplify the CODEC (VS1053) output with a single DC supply operating with 5V DC.
Suneetha.
Other Parts Discussed in Thread: TL971 , TINA-TI Dear Sir
The Spice model of TL971 downloaded from TI website includes many subcircuits, how can I use it in Cadence 16.6, or can you give me a Pspice model of TL971 which can be used in Cadence16.6…
Other Parts Discussed in Thread: TL331 , LM339 , LM393 Hi
If I am using one of these as a comparator, how long until the output comes out of saturation? I would need it to work well up to 2kHz or so.
I will have it set up for 100mV of hysteresis.…