The TS321-Q1 has exactly the same characteristics as the LM2904-Q1. But there is no -B model.
The TL971-Q1 does not have rail-to-rail inputs. If you are using input voltages near −5 V, use the TLV9151-Q1 or TLV9351-Q1.
Part Number: TL971 Other Parts Discussed in Thread: ALP , DS90UB971-Q1 971 EVMs are not being detected over USB. I have tried this with 2 971 EVMs. If we connect the 971 EVM via aardvark, we are able to detect it. Please see the snapshot below of the…
Hi Ron, I still do not understand that you said. Q1: For figure 1 and figure 2, they are differences are φM and f0. But what are the φM and f0? Q2: For figure 1 and figure 2, you mean that find gain 0dB, go vertical to phase line, then the intersection…
The OPA145 also looks like a good choice, this file has not been recently updated so the OPA196 is not in yet, and the pricing is out of date.
OPA111A options.xlsx
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…