Other Parts Discussed in Thread: TLC277 , INA114 Hi, I'm trying to simulate INA114 & TLC277 in spice, and am wondering if noise has been included for these two parts in the spice macro models for the 1Hz-100Hz region. Thank you, Abdel
Elvva,
On June 9, 2023 the design was changed. See https://www.mouser.com/PCN/Texas_Instruments_PCN20230608002_20230609175242536.pdf . The data sheet was updated to reflect the changes. old data sheet for TLC272B shows the old specifications.
Best…
Part Number: TLC2264 Other Parts Discussed in Thread: TLC2262 , TL032A , TLC277 , TL052A , TLE2027 Hi team,
Could you please help us for following 2 questions?
I referred to the page, https://e2e.ti.com/blogs_/archives/b/precisionhub/posts/ic-long…
Hi Wu,
take care, to assure that the output MOSFET goes into hard saturation, VOL at IOL=0A is specified for VID=-0.1V (differential input voltage) and for VIC=0.5V (common mode input voltage). With a much smaller VID or even a positive VID the input…
Hi Eggsy,
Kai is correct. Take a look at the "Available Options" table at the top of page 2 and the recommended operating conditions table located at the bottom of page 4 in the datasheet. When the part number has an "I" suffix it is specified to operate…
Part Number: LM741 Other Parts Discussed in Thread: TLV3701 , TLC277 , TLC271 , TLC272 , TLV271 , TLV272 , LM358 I am using a 741 as a simple comparator. Supply voltage 10V. The input voltage range is low and must be variable between 0.8V and 2.5V. I…
Hi Yildirim,
in order to achieve a symmetrical output signal I have taken a OPAmp with a low offset voltage. And in order to achieve a full output swing I have taken a OPAmp with output rail to rail ability.
For experimenting you can use the TLC277…
Hi Brian,
that problem do you have with any other CMOS-OPAmp as well and from any other manufacturer.
The datasheet of TLC272 contains a useful information:
"Because CMOS devices are susceptible to latch-up due to their inherent parasitic thyristors…
Hello Ron & Clemens,
Thank you for your feedback,
Regarding your below concern,
Do the boards pass later production tests?, >>> No, we have tried to do the further test after the ICT failure, but it is not getting pass for further tests [FVT…
Jaka,
TLC277 is offered in three different grades based on its specified temperature range which are denoted with suffix C, I, or M - please see below:
Therefore, TLC277 C DG4 with suffix C (Consumer) is specified only from 0C to 70C. If you need…