Part Number: TLC3702-Q1 Customer PN : T100000585 MPN : TLC3702QPWRQ1
Data sheet show : MSL3 for TLC3702QPWRQ1
Actual Label show : MSL1
And not ship under MBB.
It is concern part quality.
Please review and provide, Why MSL classificaton on…
Part Number: TLC3702-Q1 Other Parts Discussed in Thread: TLC3702 Tool/software: Hi,
To clarify in the very beginning.We are using a spare TLC3702QPWRQ1 in below configuration. As per this link.
Application Design Guidelines for LM339, LM393, TL331…
Part Number: TLC3702-Q1 Tool/software: Hi,
I need PSpice model of TLC3702QPWRQ1 which is modeled for considering temperature(-40 °C to 125 °C) parameter.
I want simulated my circuit using PSpice for temperature range.
Part Number: TLC3702-Q1 Other Parts Discussed in Thread: TLC3702
Hi,
As per datasheet it is recommended that the input voltage should be in range from -0.3V to VDD.
and pin current should be limited to +/-5mA.
I have to apply Automotive standard…
Part Number: TLC3702-Q1 Hi,
Can i know the Junction temperature for TLC3702QPWRQ1. Its not mentioned in the datasheet. For similar component TL331QDBVRQ1 its given as 150C. Please let me know whether Tj is limited to max ambient or its 150C for TLC3702QPWRQ1…
Other Parts Discussed in Thread: LM2903-Q1 , TLC3702-Q1 , LMV762Q-Q1 , LM2903 Dear all,
My customer is interested in TLC3702-Q1 / LMV762Q-Q1 / LM2903-Q1.
Please answer following question about these devices.
Question 1,
If we mistake and supply…
Other Parts Discussed in Thread: TLC3702-Q1 Hello,
The datasheet on page 1 under features says: Single-Supply Operation . . . 3 V to 16 V
But on page 3, V DD Supply voltage is shown to have a recommended minimum of 4V
Can this part be used with…
Harish,
Here is a comparison. I don't see any issues.
TLV1812-Q1
TLC3702-Q1
PDF data sheet
PDF data sheet
PDF data sheet
HTML data sheet
HTML data sheet
HTML data sheet
TI.com inventory
181,212
261,065…
Hello Elisha,
You can use values from the TLC3702-Q1 datasheet for the SOIC package. These numbers will be included during the next update of the TLC3702-EP datasheet.
www.ti.com/.../tlc3702-q1.pdf