Hello Pranay,
The commercial version spice model should be a good alternative.
https://www.ti.com/product/TLE2062A#design-tools-simulation
TLE2062, TLE2062A, TLE2062B PSpice Model
Hi Kai,
Earlier I had posted a question about the open loop output impedance of TLE2061 and TLE2062.
The response that I got was, TLE2061 and TLE2062 uses the same output stage so the Zo should be the same.
Thanks,
Hi user,
yes, I can confirm this. Just measured 9mA with a TLE2062 (the neighbour channel connected as voltage follower with the +input connected to 0V).
Well, the TLE2062 is an OPAmp and no comparator...
Kai
Hi Pengfei,
the OPA365 and OPA2365 need not to contain exact identical operational amplifiers. The TLE2061 and TLE2062 don't do that either, for instance. (They differ in the open loop output impedance.)
Looks like the OPA2365 limits to a lower short…
Hello Venky,
Here are some parts you may consider. They have similar or better bandwidth, maximum voltage offset, slew rate, supply current, and voltage noise specifications as the LF442CN. They are also +/-18V supply capable, like the LF442CN, and…
Part Number: TLE2062AM Other Parts Discussed in Thread: TLE2062 , TLE2022 Hi,
I am sorry but my english is very bad. Yes i am french, :) .
My problem is :
i use a TLE2062AM in converter "Voltage -Current" with a load inductive.
I am not problem…
Hi Marcoo,
the 2.8mA current consumption of the REF1933 was measured without any load at the output! Only said 2µ2_X7R_0805 load capacitance was present. Nor was it a charging current of this cap, because the measurement was pure DC. I increased the…
Other Parts Discussed in Thread: TLE2062 I would like to estimate the current consumed by my circuit in order to size the power resistors. I have 2 LOG102, 2 OPA129, and 9 TLE2062 in the circuit, as well as assorted passive components.
JD
Thanks for the suggestion. I looked at the OPA1652 datasheet and it would work very well, but I am needing the increasingly unavailable PDIP package for socketing.
I ordered TLE2082 and a TLE2062 to try
and a LM833 which has 7uS slew and 2.5mA…
The OPA145 also looks like a good choice, this file has not been recently updated so the OPA196 is not in yet, and the pricing is out of date.
OPA111A options.xlsx