Part Number: TLV1701-Q1 I have a question regarding the TLV1701QDBVRQ1 absolute max signal input levels.
The datasheet specifies that the maximum signal input voltage is (Vs+) + 0.5, and the maximum input current is ±10mA.
Note 2 also states that…
Part Number: TLV1701-Q1 Hi team,
May I ask the meaning of short circuit sink current?
Does the indicator in the red box of TLV1701-Q1 mean that the output terminal is short-circuited to the power supply, and there is a protection circuit inside to control…
Part Number: TLV1701-Q1 Other Parts Discussed in Thread: TLV1701 , TLV1704 I can not find any documentation on what process the TLV1701-Q1 is built on. Is it built on the BICOM3xHV process? If not, what process is it built on?
Part Number: TLV1701 I have downloaed TLV1701 Psipce Model (rev.B) from TI website ( https://www.ti.com/product/TLV1701 )
Open the Pspice example project (TLV1701.opj) in the downloaded file with OrCAD capture 16.6
Run the simulation and got following error…
Part Number: TLV1701 Other Parts Discussed in Thread: TIPD114 Hi Expert,
May I learn from you if customer used TLV1701 without hysteresis, how could we get estimated total threshold voltage variation for Vin+ from DS spec point of view?
Take TIPD114…
Part Number: TLV1701 Other Parts Discussed in Thread: TLV3401 , TLV3491 Hi Expert,
Could you please let me know the Propagation delay at overdrive=2mV
Thanks
Muk
Part Number: TLV1701 Other Parts Discussed in Thread: TLV7011 , TLV1805 Hi team;
1,Per the following thread, I know that the output state of TLV1701 is not garanteed, and team would do some test, could you share the test result?
https://e2e.ti.com/support…
Claudio
It is a community effort to solve problems some times. Glad it all worked out. From your emails, it sounds like I can close this thread. We will look forward to hearing from you again in the future.
Chuck
Part Number: TLV1701 Other Parts Discussed in Thread: TL331B , TLV1805 Background:
We are using the TLV1701AIDBVT comparator in conjunction with a pull-up to drive the gate of a fast FET. When the + input goes higher than the threshold on the - input,…
Part Number: TLV1701 If the TLV1701 is run from 5VDC supply, can the output be pulled up to 15V supply through a 10k resistor? Of course, when the design is updated, the device will run from a 15V supply, but this is a rework of an existing design in which…