Part Number: TLV1701 Other Parts Discussed in Thread: TL331B , TLV1805 Background:
We are using the TLV1701AIDBVT comparator in conjunction with a pull-up to drive the gate of a fast FET. When the + input goes higher than the threshold on the - input,…
Part Number: TLV1701 If the TLV1701 is run from 5VDC supply, can the output be pulled up to 15V supply through a 10k resistor? Of course, when the design is updated, the device will run from a 15V supply, but this is a rework of an existing design in which…
Part Number: TLV1701 Other Parts Discussed in Thread: TLV3201 , TLV7011 Dear Experts,
My customer is evaluating this product and wants to know more about propagation delay versus input overdrive.
Specifically, in the typical curve (figure 8), the plot starts…
Part Number: TLV1701-Q1 Other Parts Discussed in Thread: TLV1701 Hi,
I would like to know if there are any significant differences between the dies used in the different versions of the TLV170X-Q1 components. I see from the reliability report that all…
Part Number: TLV1701 Team,
can you confirm that the "input bias current" (Ib) in the datasheet specifies the maximum current that the device can draw? (20nA over full temp range)
My customer needs conformation that this is the critical value…
Part Number: TLV1701 Dear Sirs or Madams,
Please let me have the following two questions regarding Recommended Operating Condition on Supply Voltage;
Q1
The datasheet says that Minimum operational supply voltage is 2.2V, which means that TLV1701 is …
Hi Sagar,
This part doesn't cover full rail-to-rail input where the input ranges from Vee to Vcc.
LM2903B covers from Vee to Vcc - 2V, which lis likely why there are functional issues with the noninverting terminal at 2.3V.
With this setup, max recommended…
Part Number: TLV1702-Q1 Other Parts Discussed in Thread: TLV1701 Hi team,
My customer requires spice model for TLV1702-Q1.
Can we propose Pspice model of TLV1701 instead?
Best regards,
Part Number: TLV1701 Other Parts Discussed in Thread: TLV3701 Hi Team,
A customer of mine had the following question concerning the TLV1701.
The output of the TLV1701 requires a pull-up resistor. He was wondering what the max value of the pull-up resistor…