Part Number: TLV1702-Q1 Other Parts Discussed in Thread: TLV1701 Hi team,
My customer requires spice model for TLV1702-Q1.
Can we propose Pspice model of TLV1701 instead?
Best regards,
Part Number: TLV1702-Q1 Hi team,
My customer is using TLV1702-Q1. They want to know if 'Voltage Output Swing From rail' is the same spec like VOL?
And could we provide our test diagram/test circuit for this spec?
Regards
Michael
Part Number: TLV1702-Q1 Other Parts Discussed in Thread: TLV7022 , TLV7012 Hi Team,
We are looking in for AC over current sensing application of a 3 phase motor inverter.
Current transducer output is from 0.5V to 4.5V.
Over current threshold limit…
Part Number: TLV1702-Q1 Other Parts Discussed in Thread: LMV7271 Hi,
Planning to use IC TLV1702-Q1 as a analog voltage comparator. Moreover, we have variable reference adjustment (i.e. from 0.5V to 10V & -0.5V to -10V ).
Question is, How shall I adjust…
Part Number: TLV1702-Q1 Other Parts Discussed in Thread: TLV1702
The Above Circuit is Designed to satisfy below requirement:
1. HIGH FOUT When LED Is Normal
2. LOW FOUT When LED is Fail Open
3. LOW FOUT When LED is Fail Short
4. LOW FOUT When…
Part Number: TLV1702-Q1 Hi Team,
I have three question about TLV1702-Q1's output low level.
1. I Could you tell me the max Vol level?
2. Are there any equations to estimate Vol level at a temperature like 100C?
3. Could you tell me what "Voltage…
Part Number: TLV1702-Q1 Hi team,
When using only 1 channel out of 2 channels, how should I handle the unused 1 channel pins?
We are thinking the method that we will tie In+ to Vdd and In- tie to GND. The output terminal is open.
As we do not want…
Part Number: TLV1702-Q1 Other Parts Discussed in Thread: TLV1702 Hi,
TLV1702 is RRI comparator, but looking at internal structure the input stage is NPN.
Can this really guarantee that input voltage is up to the rail?
Doesn't RRI require PNP stage…
Part Number: TMS320F28069M Other Parts Discussed in Thread: TLV1702-Q1 , Hello, I'm currently designing a 3 phase inverter using instaSPIN and the LAUNCHXL-28069M. On the controls side of the design one of my design requirements is to have over-current…
Part Number: TLV1702 Other Parts Discussed in Thread: , TLV7022 We are using samples TLV1702-Q1 for our design with 5V supply and pull up resistor of 1k ohm.
Of the dual comparators, one is working fine but the second gives a high output of around 2…