Hello Jazz,
Have a look at the TLV1702-Q1. It is in the VSSOP package (you did not say which package you were using).
The TLV7022 would also be a good replacement. The Q1 version is scheduled for later this year.
Are both inputs going to be near…
Hi,
Thanks for your reply.
I am a little weak on comparators but i think i have spotted a problem.
If the LM2903 is powered by +-12V, and the input into the comparator swings between -12V to +12V. Does this therefore mean the comparator is out…
Hey Jon,
We currently have the TLV1702-Q1 , which is the 2 channel device, that is AEC-Q100 qualified. If that device does not work, go ahead and reach out to me, my information is below. We can find you the right device for your design.
Thank you…
Part Number: LM2901 Other Parts Discussed in Thread: TLV1704 , TLV1701 , LM339 , LM393
Dear Sir, please answer
There is feature description from LM2901 datasheet, page 10: "The output NPN sinks current when the positive input voltage is higher than…
Part Number: TLC393 Other Parts Discussed in Thread: TLV274 , , LMC6772 , TLV1702 , TLV3402 , LMC6484 , TLV2374
I am trying to design a thermostat and I originally used the op amp TLV274 as a comparator with some success, but I wasn't happy with the…
Hello Shu-Cheng,
The legal input voltage range is 0V to 2V below V+.
With a 5V supply, the legal input range is 0V to 3V. The values shown in the schematic are within legal range with a 5V supply.
With a 3.3V supply, the valid input range is 0 to…