Part Number: TPS40210 Other Parts Discussed in Thread: TLV172 Tool/software: WEBENCH® Design Tools I am trying to design a -24V to -15V switcher that can deliver up to 6A. Years ago Peter James Miller provided a topology which used the TPS40210 to generate…
Hi Shihab,
The OPA172 or TLV172 is where I would start, but it has higher Iq than the TLE2061AM. Can you provide a little more information on your application? What type of circuit is this? We might have offerings in both our Precision Amps and Audio…
Hi Pavithra,
Yes, full operating condition means full operating temperature range. I looked into THS4052, this part will work for you but it's a high speed part (Slew rate = 240 V/us), it's more expensive and not a similar match for LM358. Some…
Part Number: TLV170 Other Parts Discussed in Thread: TLV172 , , TLV171 In the datasheets for tlv170, tlv171, tlv172 is mentioned that " The input can operate 100 mV below the negative rail and within 2 V of the positive rail for normal operation. Note that…
Hi Ting,
The following also have the "South-East" pin-out, Vs >16V and >85°C:
OPA170
OPA171
OPA172
Note that some of these have different SOT-23 and SC-70 pinouts - so be careful which you are selecting...
At some point in the future…