Part Number: TLV1H103-SEP Other Parts Discussed in Thread: TLV1H103-SP , , LM111 , TLV3603E , TLV3603 Tool/software: The comparator I am looking at is the TLV1H103-SEP that is radiation rated for 30krad. I tried searching for -SP part (TLV1H103-SP) to…
Part Number: TLV1H103-SEP Other Parts Discussed in Thread: TLV3603 Tool/software: Hello.
Could someone please help me with a commercial equivalent part for the TLV1H103MDBVTSEP? (Non-radiation tolerant)
Thank you.
-Henk
Part Number: TLV1H103-SEP Tool/software: Hi,
I’m simulating TLV1H103-SEP in PSpice , and I’m encountering an issue when VEE is not tied to GND .
Specifically, when I apply a positive offset voltage to VEE (e.g., VEE = +1V instead of 0 for example…
Part Number: TLV1H103-SEP Tool/software: What is the additive jitter of the TLV1H103-SEP when used to drive a 50MHz clock signal? It would be driven by an LVDS-type input (350mV differential voltage).
Hello Charles,
Yes. Forcing a voltage on the HYST pin to adjust the hysteresis would be better.
See these posts:
TLV3605: Adjustable (internal) Hysteresis
TLV3605: Hysteresis control with external voltage instead of resistor
Also see the TLV1H103…
Hi Niels,
It's possible to drive the nLE/HYST pin of the TLV3603 to set the internal hysteresis.
The Hysteresis vs nLE/HYST voltage plots are currently not available on the TLV3603 datasheet, but those plots are available on page 13 of the TLV1H103…