Part Number: TLV2171 Other Parts Discussed in Thread: TLV9352 Dear team,
I have a question on TLV2171 from customer. could you pls help answer? thanks a lot.
Below ordering number on snapshot is TLV2171AIDR that customer sent. but from website I can not…
Part Number: TLV2171 Dear team,
When using TLV2171 as differential amplifier, the output pin7 was being added a 3.9V/ 59kHz sine waveform, no mater whether to have input signals.
The output range is 0-2.8V, Gain=3.3, Voltage +/-15V.
Hi Robert,
Customer want to decrease the battery quiescent consumption in the shutdown state, in this state, customer found that the battery output current is 200μA;
After increasing the circuit resisters with 5x, the current decrease to 34μA; but it…
Part Number: TLV2171 Other Parts Discussed in Thread: OPA2991 , OPA2992 , TLV9062 , OPA2834 , LMH6643
Hi team,
My customer need a faster settling time amp than TLV2171 0.1% 1μs, which used to sensing HVAC DC_link current and get higher sensing precision…
Part Number: TLV2171 Hi,
in the datasheet, the short circuit current of TLV2171 is 25mA source and 35mA sink.
And there is also a plot shows Output Voltage Swing vs Output Current in Figure 5.
Does it mean that if the output voltage swings from V+ to 0V…
Part Number: TLV2171 Hi Team
When using TLV2171 in unity gain amplifier as voltage follower as below, the voltage output goes to 13.5V, almost the same as the power supply. What kind of reason could cause such abonormal phenonmenon with a zero input. …
Part Number: TLV2171 Other Parts Discussed in Thread: OPA2991 , TLC2272 , TLV9152 Hi team,
My customer reported an issue that: TLV2171IDR output not worked as expected voltage, especially for specific comparator application, seems the negative input cost…
Part Number: TLV2171 Other Parts Discussed in Thread: TL082 Hi Team,
May I know what TLV2171 happen when it output latch? Even thought TLV2171 input signal change, output keep latch. Only power off, TLV2171 work normally.
Do you have any suggestions?
Thanks…
Part Number: TLV2171 Other Parts Discussed in Thread: LM358 , OPA2171 , INA180 My customer wants to use amps for high side current sensing in the battery application. Their challenge is that when the battery goes into sleep mode, there will be undesirable…