Other Parts Discussed in Thread: TLV2244 I'm currently in the process of modeling a device that uses the TLV2244 operational amplifier however the 2240 series is missing from all my libraries and doesn't seem to be anywhere online. Does anyone have a…
Dear Herman,
Thank you for the very prompt reply!
But in TLV2242 ds, it shows input common mode range of 0 to VCC. http://www.ti.com/lit/ds/symlink/tlv2244.pdf
May I know where I can see the CMIR 1V below VCC?
The 2IN+ connects to VCC is from…
Hello Yonatan,
I am assuming the 80uA is for all four amplifiers (20uA max per amplifier) in a "PW' (TSSOP-14) package:
GPN
VosRoomMax (mV)
IsMaxCh (mA)
GbwTyp (MHz)
1kPrice ($)
LMP2234
0.15
0.009
0.13
1.86
LPV324…
The OPA145 also looks like a good choice, this file has not been recently updated so the OPA196 is not in yet, and the pricing is out of date.
OPA111A options.xlsx
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…