Part Number: TLV2316-Q1 Dear Sirs,
My customer asked us about slew rate variations for TLVx316-Q1.
Please tell me the variation of slew rate due to process variation. I know that it is not a guaranteed value.
Best Regards,
Y.Hasebe
Part Number: TIDA-01421 Other Parts Discussed in Thread: TLV2316-Q1 , LMV7275-Q1 How the peripheral RC values(shown in red circles below) for TLV2316-Q1 and LMV7275-Q1 are calculated in the TIDA-01421 design?
Dam Hung,
I don't know what might be happening. I do suggest measuring the voltage on all the TLV2316 pin to make sure they are as expected with a new sample. Does the IC get hot before or after failing?
Shinichi-san,
Lack of temperature limits for TLV2316-Q1 is intentional. This is a transfer risk from manufacturer to customer.
Some similar devices that have temperature limits are as follows.
TLV9002-Q1 Vos (RRIO device) TL972-Q1 Vos, Ib (RRO device…
Hi Thomas and Kai,
To add more possible low cost devices (CM to ground, < 22nV/RtHz noise, > 1MHz, 20mA output current, dual), here they are:
Device
RR Out?
CM to ground?
Cost (1k units) $
LMC6032
Yes
Yes
0.35
LMV722…
Hello,
I believe the OPA2171 will meet all of the specifications you are looking for. Below I show the specifications of the OPA2171 that you mentioned you are concerned about in your post.
Minimum Supply Voltage: 2.7V Noise Density @ 1kHz: 14nV/rt…
6136.SCHEMATIC1 _ PAGE4.pdf Dear Sir,
I have also attached clear schematics for your kind reference, please check and help to provide valuable suggestions.
Aravind.
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…