Hi Alpaslan,
the negative supply voltage had the wrong polarity:
But take care, the TLV2324 is a micropower OPAmp and due to its very low speed the TLV2324 cannot achieve a high bandwidth with a gain of 500:
alpaslan.TSC
Kai
Hello Yonatan,
I am assuming the 80uA is for all four amplifiers (20uA max per amplifier) in a "PW' (TSSOP-14) package:
GPN
VosRoomMax (mV)
IsMaxCh (mA)
GbwTyp (MHz)
1kPrice ($)
LMP2234
0.15
0.009
0.13
1.86
LPV324…
The OPA145 also looks like a good choice, this file has not been recently updated so the OPA196 is not in yet, and the pricing is out of date.
OPA111A options.xlsx
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…