Part Number: TLV2464A-Q1 Hello,
I am currently reviewing the datasheet for TLV2464AQPWRG4Q1, and I noticed that thermal resistance values are not listed for the 14-TSSOP package. Could you please provide the thermal resistance specifications (thetaJA…
Part Number: TLV2464A-Q1 Please help to confirm the difference between TLV2464AQPWRQ1 and TLV2464AQPWRG4Q1.
They use the same datasheet. The only difference is the “ G4 ” in the latter component.
Can they be used to replace each other without validation…
Part Number: TLV2464A-Q1 Hi,
My clients use these two chips. What is the difference between these two chips? Can the two types of chips be used interchangeably?
Thanks!
Part Number: TLV2464A-Q1
Hi,
I would like to understand why we specify Ibias so differently in the table(pA) and in the diagram(nA!)?All are typical but the difference is so big……
Can you explain which is correct?Thanks
Umberto
The OPA145 also looks like a good choice, this file has not been recently updated so the OPA196 is not in yet, and the pricing is out of date.
OPA111A options.xlsx
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…
Hi, David,
The THD will be better, of course, but not massively better. I couldn't find any data we had taken for this.
Years ago, we did an app note on this type of system. the compensation of the op amp proved to be very difficult, so we never…