Part Number: TLV2474A 8 locations had coplanarity issues from this part. WO (1036474) qty was 960. This part is 3 per board. So 8/(960*3) *1,000,000= 2777.78 DPPM
Part Date Code is: 2308
Lot # 3148292TW3
How do I get about replaccing the parts?…
Part Number: TLV2474A-Q1 Other Parts Discussed in Thread: OPA2333 , TLV2474A , TLV9064-Q1 , OPA2333-Q1 , TLV2474-Q1 , OPA2333-HT , TLC2274-HT Hi team,
Could you recommend op amp that is pin to pin with TLV2474A-Q1 and have similar spec?
It is 4…
Part Number: TLV2474A-Q1 Hi TI,
Since this IC is a 4-channel op-amp, what termination should be made for the not use op amp channel? Should I ground the output and input of the not use channel?
Thank you.
Best regards,
Fariz
Part Number: TLV2474A-Q1 Other Parts Discussed in Thread: TLV2474 Hi,
As far as I know, TLV2474AQDRG4Q1 and TLV2474QDRG4Q1 have the same electric/mechanic specification except for Max. input offset voltage.
However, I've recently found that they…
Part Number: TLV2474A Hi Team, we have a customer that wants to confirm if there is a maximum temperature coefficient of input offset voltage. It is found on the datasheet that the value is only at typical.
Hoping for your clarification.
Thank…
Part Number: TLV2474 Tool/software: Hi ,
We are using the TLV2474A as a voltage follower to drive reference voltages of 0V to 2.5V to digital Trimpots. The current design does not have any series resistors. Because there is a large heatsink covering…
The OPA145 also looks like a good choice, this file has not been recently updated so the OPA196 is not in yet, and the pricing is out of date.
OPA111A options.xlsx
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…