Other Parts Discussed in Thread: TLV5614 , ADS7864 , TLV2548 I need to download the IBIS model for theAD,DA convertor for a simulation of my prototype circuit board.
I checked it on TI homepage , but the link of ibis model was not described.
If you…
Part Number: TLV2548 Hi All,
I lately use TLV2548 to get the Sin and Cos signals. The ch2 is used to achive Cos, and the getted signal is right.But the Sin signal is not right, which is getted by ch0. As show below,when the signal is bigger than some…
Part Number: OPA211-EP Other Parts Discussed in Thread: TLV2548-EP , Hi Team,
I have question about how to select a buffer amplifier for TLV2548-EP. I used Analog engineer's Calculator and input some spec of the TLV2548-EP.
Could you check my filling…
Part Number: OPA340 Other Parts Discussed in Thread: TLV2548 , Hi,
I have a OP340 in non-inverting configuration driving into a TLV2548 ADC. At lower steady state amp input voltages (in the region of 0.65V) I'm see an oscillation at the output of the…
Part Number: TLV2548-EP Hello,
My customer has aquestion about TLV2548-EP.
[Q]
What is the ESD voltage of TLV2548-EP? (HBM and CDM)
Best Regards,
Kaede Kudo
Part Number: TLV2548-EP How do I Set the timing for the CS signal WRT SCLK? The recommended operating conditions suggests that the delay from the 16th falling edge of SCLK to the rising edge of CS should be a minimum of 0.5 SCLKs, which means (I think…
Hi,
Thank you for helping me so patient. My problems has already solved. The problem is the input signal' speed shoudn't exceed the AD‘ speed. The TLV2548's speed is 80KHz in my design. So the input signal should not exceed 8KHz, or the transition will…
Fikadu,
We will close the thread for now. If you do not reply within 30 days, the thread will lock. You can then click the "Ask a related question" button, which will create a new thread but add a link to this one.
Regards,
Mark
Part Number: TLV2548-EP Here is the customer’s question:
Right now we have FS tied high and use STE as /CS. (called FS=1 mode) We would like to tied /CS permanently low and use STE as FS. The short STE pulse gives us better control of the ADC start…
Part Number: TLV2548-EP Other Parts Discussed in Thread: TLV2548 Hi Support team,
Customer has a question on timing, page 19 in the EP data sheet and figure 20 in data sheet, td(SCLK–DOV)
His comments:
I have the TLV2548 configured for FS = 1…