Other Parts Discussed in Thread: TLV3012 The TLV3012 is rated for up to 10nF capacitive load on the reference terminal.
What is the minimum output series resistance that I need to drive 100nF load without oscillation?
Peter
Part Number: TLV3011 Other Parts Discussed in Thread: TLV3012 , TINA-TI Hello,
Devices concerned:
TLV3011 and TLV3012
Datasheet used:
SBOS300B – FEBRUARY 2004 – REVISED JUNE 2004
Question:
Do you have data about input bias and offset…
Hi Abe,
I am glad that the excel tool helped.
In regards to your question, it sounds like you don't intend on using an external reference. Thus, I recommend using the TLV3012 with a 1.242V internal reference. It is a push-pull device as well so there…
Hello,
Thank you for the link to op-amp parts with integrated reference voltage.
In fact, my technical needs are listed below :
Automotive qualified part (AEC-Q100 mandatory)
Operating from a +12Volts battery supply (range +8,0Volts to +35Volts)
No…
Part Number: TLV3691 Other Parts Discussed in Thread: TLV4031 , TLV4051 , TLV4021 , TLV4041 , TLV6703 , TLV3011 , TLV3012 Hi team,
My customer is looking for a comparator which support 1.8V to 5.5V Vcc, Vref=1.2V and package is preferred to be DFN1.6*1.6(not…
Hi Goran, I am Manuel Chavez, a colleague of Koteshwar's. Gate capacitance of PMV30XPEA might be too high for TLV3012 to drive, so the P-FET may be continuously shorting +3V3-ISO3 to 0V-ISO3. Can you attempt to use DMP3056L instead? Thank you, Manuel…
Part Number: TLV3404 Other Parts Discussed in Thread: OPA348 , TLV3012 Hi,
With the support from this forum I have been working on a design of a 2 stage op-amp design. This design uses an OPA348 and a TLV3012. Purpose of the design is to detect the signal…
Part Number: TLV3011 Other Parts Discussed in Thread: TLV3012 It looks like the hysteresis calculation in Figure 2 / June 2004 datasheet is incorrect - I calculate 0.33 V instead of 0.38V (assuming a low value pull-up or the TLV3012 push-pull output - please…
Part Number: LM2904-Q1 Other Parts Discussed in Thread: TLV313-Q1 , TLV3011 , TLV3012-Q1 Hi team,
Could you please help to check if we have automotive qualified opamp to replace SGM321YC5 and SGM8710? Better to have P2P solution.
Thanks!
Hi Jeroen,
based on the piezo signal modelled by Paul if have created and simulated the following circuit:
It uses another OPAmp, the OPA348. As comparator the TLV3012 was chosen, because it contains a stable voltage reference, which might be useful…