Part Number: TLV3012B-Q1 Other Parts Discussed in Thread: TLV3012 Hi,
I am using a TLV3012 comparator with its push-pull output directly driving the gate of an IRLML6402 PMOS through a 100 ohm series gate resistor.
I am trying to determine whether…
Part Number: TLV3012-Q1 Other Parts Discussed in Thread: TLV3012 Hi all.
We use TLV3012AQDCKRQ1 (i.e. TLV3012-Q1 / SC-70 footprint).
Does this comparator has clamping diodes at its inputs?
It looks like it has calamping diodes due to absolute…
Hi Amod,
To show the behavior you intent to design:
1. Analysis -> DC Analysis -> DC transfer Characteristic
2. On the GUI of DC Transfer Characteristic, change "Input" from R1 -> V2
This is because you're sweeping against input generator/voltage…
Part Number: TLV3012-Q1 Other Parts Discussed in Thread: TLV3012
TLV3012AQDCKRQ1
TLV3702QDRG4Q1
TL331QDBVRQ1
For these three Comparators, the ESD ratings have been omitted from the most recent datasheets, even though the Qualification Summary…
Part Number: TLV6700-Q1 Other Parts Discussed in Thread: TLV3012-Q1 , TLV3011-Q1 , TLV3012B-Q1 , TLV3011B-Q1
Do you have a alternative for the TLV6700-Q1, where the interal voltage referenz is routet to a pin/ can be monitured? I need basecly a window…
Hello,
Thank you for the link to op-amp parts with integrated reference voltage.
In fact, my technical needs are listed below :
Automotive qualified part (AEC-Q100 mandatory)
Operating from a +12Volts battery supply (range +8,0Volts to …
So sorry for our delayed response.
this device is functional safety capably only and I have provided a report showing Fit Rate numbers and FMD
Chuck
FIT and Failure Mode Distribution TLV3012B-Q1.pdf
Part Number: TLV3012 Other Parts Discussed in Thread: TLV4021 , LMP7300 , INA206 , TSM102 , LMV7231 Hello,
I'm considering using TLV3012-Q1 in a design. I do not have any issues with it so far, but I did notice it is a bit older. Is this the best part…
Unfortunately only the push pull version, tlv3012-q1 is auto qualified. Does the application really require the level shifting function of the open drain output or are the ORing two open drain outputs together? If not, maybe they could use the push pull…
Hi Jared,
There is a comparator product that meets all but the last of the requirements, the TLV3012A-Q1. I copied some information from its datasheet:
Push-pull output
Input Common-Mode Range 200 mV beyond supply rails
Voltage reference, 1…