Part Number: TLV3201 Hi there,
Could you inform me about terminal finish of the part TLV3201AIDBVR. Also, could you tell me the thickness of Au in case the terminal finish is NiPdAu or NiAu or Au.
Thanks.
Best Regards,
Kaoutar Ben Kaddour
Part Number: TLV3201 Hello. I have scoured the data sheet (I think) and the web but I cannot find any statement that indicates whether the output of the TLV3201 is CMOS or bipolar.
Can someone please point me to the documentation that states this?
Thank…
Part Number: TLV3201 Hi i want to sense grid voltage and cutoff operation with hysteresis band using TLV3201
i designed with 185V ac ON and 175V ac off,Hysteresis band is almost 400mV
when i tried testing UV opamp alone,ON happens at 210V AC and off…
Part Number: TLV3201-Q1 I am currently refereing to SNOAA40 Application Report.
If my Vcc=5V , And below is my requirement for current threashold.
DESCRIPTION
IG1 (A)
INA-OUT (V)-> [ Vref+(Amp Gain)(IG1*Shunt Value)]
VH, CHB
Overcurrent threshold…
Part Number: TLV3201 Other Parts Discussed in Thread: TLV7011 , LMV7239 , TLV3603 Hi.
I need a comparator for a capacitor value measurement application with relaxation osc. I found TLV3201, TLV7011 , TLV3603 and LMV7239. It has to push-pull output.
I need…
Part Number: TLV3201-Q1 Other Parts Discussed in Thread: TLV3201 Hello,
I have a question about Fig 25 from the TLV3201-Q1 datasheet. It seems the intent is to show that input voltages on either the IN+ or IN- pins of the device that exceed the rails…
Part Number: TLV3201 Hello,
I have connected the output pin of TLV3201 to drive an Opto-Coupler. The idea is to calculate the resistor value to be placed between output pin and Opto (Current range driving opto 5mA ~ 20mA).
1. Should i Refer to figure…
Part Number: TLV3201 VG1, VG2, VG3 are 3 phase AC source, with an input signal voltage varying from 1V to 2.9V. VG4, VG5, VG6 are 100mv(1000Hz) added to introduce noise.
I'm calculating zero crossing with reference to line 2(Reference) in the given circuit…
Part Number: TLV3201 Hi Team,
Can you help review the schematic and calculation below? Please let me know if anything wrong.
<1k & 10k>
Vhys = 5V * 1k/(1k+10k) = 0.45V
Vutp = 0.45V*2.5V*2.5V = 2.8V (eq (4) in datasheet)
Vltp = 2.8V - 0.45V = …
Part Number: TLV3201 As per the simulation file SBOC515(Tina simulation), Noise is generated on a triangular waveform, how do generate noise on a sinusoidal waveform? what parameters or what script to write? please guide.
below is script written for…