Hi Michael,
There has been a glitch in a back-end system that caused most of the comparator datasheets to disappear from the web. We are trying to restore them at this moment.
Please see attached:
. /cfs-file/__key/communityserver-discussions-components…
Hi, Please keep me posted about the TPS3701 datasheet error issue. I want to use it for creating a over current trip signal for a current sense signal from a hall sensor. Thus, propagation delay must be kept to a minimum. It would be great if you could…
Part Number: TLV3502-Q1 Other Parts Discussed in Thread: TLV3502 , TLV3202 , TINA-TI I am using TLV3502 for fast voltage detections.
- One is for level only
- the second one is for fast zero crossing detection.
Is my circuit ok?...Including polarity…
Hello,
Thanks you for pointing out this topic, the correct circuit and formula is provided in the attached 2016 revision of the datasheet, SBOS561B-REVISED DECEMBER 2016. We will update the section of the SBOS856-FEBRUARY 2017 datasheet in a new revision…
Thank you, Kai
In the attached PRELIMINARY schematic portion, U1 is my INA180A1 current sense amplifier. Q16 emitter is connected to a 20V0 voltage reference. The current sense resistor is R49 (not shown but I label the connections to U1 pins 3 and…
Hello Hirotaka,
No. 0V and 5V will not damage the inputs. Differential Abs Max is ±5V. But the output condition may not be correct at those levels.
As you saw, the input range limits are (V+) - 2V and (V-) + 1V. The "Common Mode Limits" graphs show…
Part Number: LM2901 Other Parts Discussed in Thread: TLV1704 , TLV1701 , LM339 , LM393
Dear Sir, please answer
There is feature description from LM2901 datasheet, page 10: "The output NPN sinks current when the positive input voltage is higher than…