Part Number: TLV3404 Tool/software: Does the TLV3404 comparator have built in hysteresis? The application schematic in the datasheet does not show the hysteresis resistor.
What is the recommended value of the output pull up resistor and the hysteresis…
Part Number: TLV3404 Other Parts Discussed in Thread: TLV1851 , , LM239 Looking at Figure 4, is this part generally a bad choice if the output pull-up voltage is 1.8V?
If so,what part would be recommended that would also be compatible with higher pull…
Part Number: TLV3404 Team,
I think I found a datasheet error. Chapter 8.3.1 on page 12:
I think the dual/split supply should be ±1.25 V to ±8V instead of 16V.
Best regards
Part Number: TLV3404 Other Parts Discussed in Thread: LM7705 Team,
my customer wants to use TLV3404IPWR in a new design. The device is powered with Vcc=12V and GND = 0V. IN+ is fixed at 3V.
IN- can be exposed to a transient condition and reach -17V…
Part Number: TLV3404 Hello,
I have a question about the difference between two TI comparators: TLV3404IPWR and TLV3404IPWR G4 and can not find any specific spec or information on their differences, and it seems that they are using the same spec TLV3404…
Hi Laetitia,
I agree with Chuck. The clear answer is: You must never violate the specified absolute maximum ratings, not even very briefly!
In a 500µs overvoltage pulse is enough energy to totally destroy the chip and to cause latch-up. So, it's…
Hi Jeroen,
have you a link to the datasheet of piezo cable?
I would still add a protection and filtering scheme to the input of first OPAmp.
By the way, the TLV3404 is a quad comparator. It's not an OPAamp.
Kai
Other Parts Discussed in Thread: TPS60403 , ISO7521C , TLV3404 , TLV3401 , TPS60402 , TPS60401 , TPS60400 Looking to do simulations on PSpice, I need OrCAD symbols and PSpice model for the TPS60403, TPS7325, TLV3404 and ISO7521C and I have not been able…