Part Number: TLV3492TLV3492AMDREP is a last time buy part, alteranates like TLV3492AIDR list their min operating temperature as -40 deg C, my application needs -55 deg C as mininimum operating temperature. will the sensor support that? If not what qualification…
Part Number: TLV3492 Hi Thomas Kuehl,
i read your answer about protecting the input device P/N:TLV3492 with zener diode,my question is how can i be sure that the zener diode first work before the device?
BR,
Part Number: TLV3492 Some time ago, I measured the startup time of the TLV3492AIDCNT to be about 1 ms. We now have a number of parts that take 3-25 seconds to generate a valid output after power up. I've verified good power and inputs. Some devices start…
Part Number: TLV3492 Dears
For the TLV3492 data, there only have the TYP value for the Propagation delay time, low-to-high and Propagation delay time, high-to-low, but My customer want to know if we have the Min and Max spec for this two parameters…
Part Number: TLV3492 Other Parts Discussed in Thread: LM321 , TLV7041 , TLV7031 , LPV821 Hi,
I am looking for a compact circuit that will run on coin cell battery (power constrained app)
- need to measure a voltage a current sense resistor placed…
Hi Silviu,
The TLV3492 is one of the products where the maximum specified operating voltage, and the absolute maximum supply voltage, are the same in the data sheet. This is not an error, but the way the product development team decided to specify them…
Other Parts Discussed in Thread: TLV3492 Hi to all.
I would nedd to use a tlv3492 with 5V single supply.
I would like to know in which way could I protect inputs from a voltage up to +25V and -25V.
thanx
Maurice
Hi Brian,
There isn't a dual of the TLV3691, but there are other dual, very low power comparators having push-pull outputs. Take a look at the TLV3492 and TLV3702:
Let us know if you have any questions.
Regards, Thomas
PA - Linear Applications…
Hello Mr. ^2,
Have a look at the "DCN" packaged devices like TLV3492 or TLV3502. These are duals in 8-pin SOT-sized packages.
They are at the extremes of the LMC7211 - one is nanopower (slow) and one is fast - so you may have to trade power or speed…
Other Parts Discussed in Thread: LMV762 , TLV3492 Hello,
Although the two comparators of LMV762 are built on the same chip, their behaviour is not similar in our circuit. When the temperature drops below approx. +5 degC, one of the comparators (pin…