Part Number: TLV3501A-Q1 Other Parts Discussed in Thread: TLV3501 I have used the PSPICE model of TLV3501 comparator given in the website for simulation in LT SPICE. Can you please tell me whether this model considered all the errors(offset error, offset…
Part Number: TLV3501A-Q1 Tool/software: Hi team,
What is the maximum output current for TLV3501A-Q1?
We only find output short circuit current in datasheet, and would like to know the maximum output current when output is high
BR,
Ethan
Part Number: TLV3501A-Q1 Other Parts Discussed in Thread: TLV3501 , LMV7219 , LM111 , LM119 , TLV1701 , LM139-SP , TLV1704-SEP , LM2903B , LM2903 Hello,
What is the technology (CMOS or Bipolar) of the TLV3501AQDBVRQ1?
If it is CMOS based, would you…
Part Number: TLV3501A-Q1 Other Parts Discussed in Thread: TLV9051 , TLV7031-Q1 Tool/software: Hi,
RT is NTC (TSM1D472H3953R01-8), the resistance value decreases as the temperature increases, requires the NTC to reach 85℃ ~ 100℃, the output low level…
Part Number: TLV3501A-Q1 Other Parts Discussed in Thread: TLV3501 Hi
while using this chip in one of our boards, we notice that the SHDN does not function as excepted. in order to be sure we designed a simple test board:
in this design pin 1 …
Part Number: TLV3501A-Q1 Hello,
We’re starting verification that all semiconductor components TLV3501A-Q1 have ISO 26262 according to attached GS95033-1.
Please review and confirm for below parts.
Thanks
Evgeny
Part Number: TLV3501A-Q1 Other Parts Discussed in Thread: TLV3501 hi
I am simulating tlv3501 with Pspice.
The OrCad version I am using is 16.5.
As follows.
_____________________________________________________________________
Simulation…
Part Number: TLV3501A-Q1 I'm trying to determine the distance between the bottom of the foot (seating plane) and the top of the lead for VPN TLV3501AQDBVRQ1. If TI would specify this dimension on all of your drawings it would save me a lot of work getting…
Part Number: TLV3501A-Q1 Other Parts Discussed in Thread: TLV3201 , TLV3501
Why does the quiescent current of these two comparators(TLV3501A, TLV320x) have so huge difference?
TLV3501A: 3.2mA
TLV320x: 40uA