Part Number: OPA690 Other Parts Discussed in Thread: TINA-TI , TLV3541 , OPA357 , OPA354 Tool/software: Hi,
I’m currently designing a hardware comparator circuit that generates a fault signal to the MCU based on current thresholds. The input to this…
Part Number: PCM9211 Other Parts Discussed in Thread: DS89C21 , TLV3541 , THVD1452 Dear Sir or Madam,
i would like to convert the audio output signal at MPO0 (Pin15) of the PCM to a signal according to the AES3 standard. My configuration looks like…
Part Number: LM7171 Other Parts Discussed in Thread: LM7705 , TLV3541 , OPA365 I suppose this is a more broad question about operating dual supply OPAMPS with a single supply. I have a signal from a current transformer of 1MHz frequency and 3V peak value…
Part Number: OPA847 Other Parts Discussed in Thread: OPA843 , TLV3541 , , OPA857 , OPA855 Hi, TI team,
I have study some datasheet of op amp, such as OPA847, OPA843, TLV3541, which are configured as a trans-impedance amplifier for amplifying the light…
Part Number: OPA838 Other Parts Discussed in Thread: TLV3541
Hi,
I'm using TI's op-amps (OPA838 7V/V + TLV3541 1.3V/V) as two-stage amplifier for a current signal. The schematic is shown as following. The amplified signal goes to a MAX comparator…
Hi Zak,
Thanks for the detailed feedback.
I will be connecting the PCM9211 to an MCU, which will accept SPDIF and converts it to I2S, and MCU will be connected to a stereo DAC. (216kHz is enough)
*I'm trying to make the MCU act as an audio hub…
Hi Simon,
If you want to transmit the signal differentially then you may consider a fully-differential amplifier like the THS4551 to do the singled-ended to differential conversion and provide the power gain you need.
If you plan to transmit single…
Hi Sean
Thank you for the quick reply. The minimum BW is 170 MHz.
Are there Application Notes to outline how to implement the input filter ?
Looking at the portfolio: OPA656 and TLV3541 (EMI hardened) might be alternate candidates to suggest.
…