Part Number: TLV3691
Hello Team,
We are evaluating TLV3691 in a battery-powered application with a 3 V supply. The signal current is only several tens to hundreds of nA, so input bias current is a critical parameter.
In Figure 2 of the datasheet…
Part Number: TLV3691 I have a board where to save power I power-down the section of the circuitry that includes the TLV3691.
This results in several pins of the unpowered TLV3691 having voltages on them, as follows: #1 - The positive input can have…
Part Number: TLV3691 Hello Team,
My customer wants to use TLV3691 for a non-inverting trigger application. According to the loading or the unloading of capacitance, to apply threshold in order to get a binary signal. They would like to know the CIN…
Part Number: TLV3691 Hello,
We are testing with the TLV3691 and seeing rise and fall times much faster than expected from datasheet table 6.6.
We're seeing a 8usec delay High to Low in this o-scope shot (below) when we would expect something closer…
Part Number: TLV3691 Tool/software: Hi Team,
I am doing RS testing which is applying external noise.
our test is following standard 60601-1-2 table 4, which is 10V/m will be applied.
during that test, once the frequency reached to 600MHz, the…
Part Number: TLV3691 Hello,
I have a question about TLV3691 or really any voltage comparator that offers some type of over-voltage protection on the inputs. I have drawn a rough sketch of what I am trying to achieve. VCC supply needs to be capable of…
Part Number: TLV3691 I have a simple circuit where we are normally pulling the - input to supply. (1.8V) through a 1.5Meg resistor. The circuit is used to detect the connection of a battery module.
The - input of the comparator pulls enough current…
Part Number: TLV3691 Please disregard the previous post on this issue. I pasted in the incorrect circuit. This post has the correct circuit.
I have a simple circuit where we are normally pulling the - input to supply. (1.8V) through a 1.5Meg resistor…
Part Number: TLV3691 Other Parts Discussed in Thread: TLV7031 , TLV7011 Hi,
I am using TLV3691IDPFR as an inverter to convert 3.3V to 0V or 0V to 5V. MCU MSP430F2274MRHATEP provides TTL control between 3.3V and 0V to feed TLV3691IDPFR. TLV3691IDPFR…
Part Number: TLV3691 Other Parts Discussed in Thread: TLV7031
I use TLV3691 in a classic inverting comparator: when it is dark, the output is high, when it is light, the output is low. It is found that the circuit take a very long time (5 millisecond…