Part Number: TLV3701-Q1 Hi team,
I am not able to find TLV1805QDBVRQ1 Tape and Reel Information from the official spec.
My customer need this information. An example of this is shown below. Can you help to provide related information?
Best Regards,
Amy…
Part Number: TLV3701-Q1 Hi, team,
I have one question about TLV3701-Q1. What is Icc spec when output state LOW? Only considering IC's Icc consumption.
Thanks.
Johnny
Part Number: TLV3701-Q1 Other Parts Discussed in Thread: TLV3701 Hello,
I am using TLV3701-Q1 as comparator circuit. Please find the circuit attached.
Here the 12V is from battery. So I have to consider reverse battery condition for this design. I have…
Part Number: TLV3701-EP Other Parts Discussed in Thread: TLV3701-Q1 , OPA171-Q1 , , TLV3701 , TLV3702 , TLV2464 , SN74LVC1G66-Q1 , TS5A3159 I use TLV3701-EP to convert open-gnd connection to 5V logic level. I have 4 of these comparator circuits on the card, and…
Part Number: TLV3701-Q1 Other Parts Discussed in Thread: TLV3701 , The TLV3701 datasheet states startup time (Tsu) is up to 30mS from when the supply reaches VCC Min.
The TLV3701-Q1 datasheet does not mention this parameter. Can I therefore assume the -Q1 …
Part Number: TLV3701
Please tell me if the TLV3701QDBVRQ1 has hysteresis function.
Can you achieve hysteresis using the above method?
Thanks
Best regards,
Junlong
Part Number: TLV3701 I am interested in using the TLV3701 in a thermistor monitoring application. Given the supply rails I have available, I have different supply rails for the input signals and the device Vdd. I have two questions about operating the…
Part Number: TLV3701 Other Parts Discussed in Thread: TLV3201 TLV3701QDBVRQ1 Comparator on +5V PSU is not working correctly, tested 3 of them which has strange output
Pin 4 (-VE) = +2.5V
Pin 3 (+VE) = +0.2V
I get 5V O/P which should be 0V !.
It toggles…
Part Number: TLV3701 For part number TLV3701IDBVR, no G4 suffix, I would assume that the part is a green, RoHS compliant, part like the SN74AHC14DR. Is there a date code related to part number TLV3701IDBVR after which it can be assumed to be green?
Other Parts Discussed in Thread: TLV3701 Hello Team,
The TLV3701 datasheet does not report information on the typical ESD protection characteristics (voltage and current).
Since the TLV3701 is a very low power device I'm not sure which ESD diode structure…