Part Number: TLV3801 Other Parts Discussed in Thread: TLV3811 Tool/software: Hello,
My problem is that the output of the TLV3801 switches like crazy (several MHz) when the voltage on In+ is the same as on in-. Unfortunately this condition is unavoidable…
Part Number: TLV3801 MPN TLV3801DSGT (IC COMPARATOR 1 GEN PUR 8WSON) is resulting in a 40% failure rate after being manually probed during the test, per our procedure.
The rate used to be around 5% in recent builds.
Two were used, on our board, per…
Part Number: TLV3801 Other Parts Discussed in Thread: SN74AUC74 Hello everyone,
I am currently trying to develop a circuit that uses a TLV3801. To simulate the components I am using LTSpice. The basic idea is to feed the non-inverting input of the TLV3801…
Part Number: TLV3801 How I would know if TI ICs are washable after assembled on a board, or not? Two ICs I have that I couldn't find any helpful information in this regard; TLV3801DSGT and TLV3801.
I even looked at the packaging datasheet which was…
Part Number: TLV3801 Hello,
I have got a question regarding the TLV3801.
We want to detect very small and very fast pulses. Height about 5 mV, length a few ns. The TLV3801DSGT seems to be perfectly suited for this task.
We see two solutions:
1…
Part Number: TLV3801 Tool/software: Hello,
What is the approximate input impedance for the TLV3801. I do not believe this information is in the data sheet.
Thanks.
Part Number: TLV3801 Other Parts Discussed in Thread: TLV3501 , Hi, I designed the fundamental circuit for TLV3501, but the output voltage was 350 mV and 250 mV for Q and Q bar output. The simulation and Instruction all said it should be 1.08 V and 1…
Part Number: TLV3801 Hello,
About the TLV3801 in the WSON (DSG0008B) package,
Could you tell me if there is a thermal problem with the thermal pad being connected to the VEE but not to the inner layer?
Best Regards,
Part Number: TLV3801 Hello TI,
Is it possible to get an unencrypted version of TLV3801 simulation model?
I understand NDA would be required.
Regards,
Dimo