Part Number: MC3303 Other Parts Discussed in Thread: TLV4170 , Dear Sir/Mam,
Good day..!!
I'm having doubt on MC3303D, Low power operational amplifier it have max , output current at load & total response time ?
With Regards,
Nivetha A., …
Part Number: ADC0808-N Other Parts Discussed in Thread: TLV4170 I am troubleshooting an issue on a design that uses an ADC0808-N. One observation I have made is that I get different behavior depending on whether I apply voltage to the VCC pin before VREF…
Ben,
Yes; pin 11 is ground for application. Vref can be also be ground, because VOUT = (IN+ - IN-) *1 + Vref.
Note that VOUT may not go lower than 0.7V due to the current demand of the feedback resistors. This would not happen on a different amplifier…
Hello David,
No problem!
There's no reason that I can think of why the TLV2464 would not work when connected as an instrumentation amplifier. I suggested the TLV4170 as an alternate due to price and it's on a newer process.
Perhaps another…
Part Number: OPA170 Other Parts Discussed in Thread: TINA-TI , TLV8801 , , TLV170 , LM2903 , TLV4170 Tool/software: TINA-TI or Spice Models Dear Sir, please answer
I used OPA170AIDR, please, see attach.
Input signal source - signal from current transformer…
Suleiman,
I think the biggest issue is that the 1k voltage dividers will pass current so that will disrupt seeing the device current on the 10k resistor.
TL084 does require up to 4V above the negative power rail (-5V) for input minimum which will be…