Part Number: TLV4314-Q1
Hi Team,
What is TLV4314-Q1 bandwidth change over temperature -(40°C to +125°C)
Mosly I'm interested in the min. value of GBW guaranteed over this temp range.
Piotr
Part Number: TLV4314-Q1
Hi,
I was not able to locate the supply current or Icc for TLV4314QPWRQ1 in datasheet.
Also for calculating the power dissipation, can I consider the following:
Iq = 250uA/ch --> Iq_total = 4*250uA
Ibias = 1pA --…
Part Number: TLV4314 Hello,
Please tell me about the contents of the notation "IPWR" at the end of TLV4314 IPWR. I think PW is a package and R is a large reel product. What is I?
or Do you have something written in a document?
Best Regards, DDd…
Part Number: TLV6004 Other Parts Discussed in Thread: LMP7716 , TLV4314 , TLV6002 , Dear Specialists,
My customer is considering TLV6002, TLV4314 and LMP7716, and have questions.
I would be grateful, if you could advise.
---
I would like to use…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…