Hi Anthony,
The TLV6700 should be better since your input voltages are within the specified input range.
We have not had any reports of latch-up on the TLV6700 when operated within the specified input range.
If you are satisfied with your answer, please…
Hello Max, Can you tell me which specs are the ones you are focused on to help us narrow it down? I can recommend some parts that are wide supply range with an internal 400 mV reference and internal hysteresis. If you could help me narrow down what specs…
Toshihiro-san,
This part operates a little funny when applying hysteresis to it. Not only does it set the amount of hysteresis at the trip point, it also offsets the trip point which is why the circuit design seems to not match the results. I'm working…
Hi Erik,
Sorry for the late response. I did some digging up of the old design files and I found that the way the part implements hysteresis is that not only does it set the amount of hysteresis at the trip point, it also offsets it as well which is why…
Dustin
You can use a window comparator to create a narrow band where the output is low or high (your choice) and the output is the inversion of that when the input is above the window or below the window. The window size is mostly determined by the accuracy…
A0: You change the three resistors to set the thresholds. The TLV6700 is the tighter-spec version of the TPS3700.
This cookbook circuit will show you how to calculate the resistor values for a window comparator:
www.ti.com/.../snva832
(The TLV6710…
Kevin,
The TLV6700 would be a great option to consider for this window comparator application.
I have also sent you an email offline about another part you can consider (not released yet).
Feel free to close this thread if you wish to continue to discuss…
For general usage case of a comparator with integrated reference, I would recommend the TLV3011 and TLV3012 which have a 1.2V integrated reference and open-drain or push-pull output stage. If you ever need higher operating voltage, we have the TLV6703…
Part Number: TLV6703 Other Parts Discussed in Thread: TLV6710 , Team,
-Is it possible to use the TLV6710 TINA model for simulating the TLV6703? -The overall electrical specs are very close so I guess that it could be realistic to do so. What do you think…