Part Number: TLV6710 Tool/software: Hello,
We're trying to use the tlv6710 and are encountering some issues.
I've also read some forum discussions and I'm pointing out that the INA+ should not exceed 1.7 V.
I downloaded the tlv6710 model and…
Part Number: TLV6710 I have designed a circuit with TLV6710DDCR IC to control the charging cycle of a coin cell battery MS621FE. The resistor combination has been chosen to meet the target voltage of Vmon(OV): 3.01V and Vmon(UV):2.01V (R1: 604K, R2:49…
Part Number: TLV6710 Hello,
The absolute max. rating of the output is -0.3V
I suppose that this means that there is a diode that clamps negative voltages.
What is maximum current this diode can accept?
Thanks
Part Number: TLV6710 Other Parts Discussed in Thread: TINA-TI Hi, I'm not able to get the correct resistor values based on my understanding of the parameters of this device.
My requirements: TLV6710 configured as Window comparator with OutA and B tied…
Part Number: TLV6710 Other Parts Discussed in Thread: TLV6700 , TLV4021 , TLV4011 , TLV4062 Here is a circuit that we use:
The problem we see is that when the zener diode, D50, is conducting causing about ~3.5V on the input U11-4 and there is a transient…
Part Number: TLV6710
I am using 2 TLV6710 ICs to provide undervoltage disconnect for a Battery operated Bipolar 6V supply. In my (LTSpice) simulation the TLV6710 monitoring the positive rail works perfectly.
I plan to use the TLV6710 that monitors…
Part Number: TLV6710 Hi,
I am reaching out to you in regards to the TI TLV6710DDCT window comparator. I was running some tests on it today so the comparator monitors the same voltage as VDD. When doing this, OUTA acted as planned and had no issues,…
Part Number: TLV6710 Good morning, I would like to use TLV6710 as window comparator in order to detect undervoltage and overvoltage on a 24V voltage supply. Undervoltage must be set at 19V and overvoltage at 36V.
I would like to supply the comparator…
Part Number: TLV6710 Hi,
Could you please let me know how treat unused pin? I will use INB and OUTP and not use INA and OUTA. In this case, Can INA and OUTA leave open or should be pull down or pull up?
Regards, Nagata.
Part Number: TLV6710 Other Parts Discussed in Thread: TL431 , TLV1805 Hi Experts,
I want to use a comparator device with high supply voltage, my supply voltage is 40V, but the maximum supply voltage of TI comparators is 36V, the device is TLV6710. …