Part Number: TPS3701 Other Parts Discussed in Thread: TLV6710 , , TLV6703 , TPS3710 Hello,
I need to replace TPS3701 with TLV6710 since the former is out of stock at all major distributors. I have done a basic comparison and have found TLV6710 as a…
Part Number: TLV6710 Other Parts Discussed in Thread: TLV6713 , Datasheet, April 2018, indicates absolute max VOUTA, VOUTB +28 V but in other places it suggests VOUTA, VOUTB nominal to be 36V. Which is correct and should absolute max = +40V?
Part Number: TLV6710 Hello,
I am using TLV6710 comparator, my normal supply to VDD is 24V, but sometimes this VDD supply can be 0V at abnormal state, and Vin will be about 1V input at this condition.
So I want to know if there is any potential risk…
Part Number: LM2903 Other Parts Discussed in Thread: AMC22C12 , TLV6710 , TLV4082 Hi Team,
Do we have a Comparator can be used for AC current protection? Like AMC22C12, but without the isolation barrier? If not, whether 2-channel input Comparator can…
Yanni
Another option would be to use the TLV6710 which is the window comparator version of the TLV6713. The unused non-inverting configuration can be put in a fixed output state while the inverting configuration can be used for the use case you described…
Hi TS,
in addition to what Paul mentioned, if the customer is looking to configure the dual comparator as a window comparator and if p2p replacement is not important, then they should look at the TLV6710
thanks Tushar
Vinayak
is the plan to monitor the line voltage directly or is there an option to resistor divide down the voltages?
we have two window comparator devices in our portfolio. The TLV6700 can operate from supplies up to 18V and the TLV6710 can operate…
A0: You change the three resistors to set the thresholds. The TLV6700 is the tighter-spec version of the TPS3700.
This cookbook circuit will show you how to calculate the resistor values for a window comparator:
www.ti.com/.../snva832
(The TLV6710…