Part Number: TLV7021 Hi,
Please kindly provide the cadence design file for LM7021, we can't serach in the Ultra Librarian:
The below design file is our request, thanks.
Part Number: TLV7021 Hi
The TLV7021DPWR is used to determine if the 1.05V supply is correctly generated for power sequencing control; the comparator should output low when the 1.05V rail is functioning normally. In the circuit design, +VREG3V3 is energized…
Part Number: TLV7021 Tool/software: Hi team,
Can you please share the information of TI internal code info of sympol such as fab, AT, date,...,etc?
Regards,
Hayashi
Part Number: TLV7021 Tool/software: I request anybody to please provide with the spice model files for the above mentioned component.I would be requiring it for a project for designing a dying gasp.
Part Number: TLV7021 Tool/software: Hi team,
Could you explain that what the via in center pad can improve?
"To reduce PCB fabrication cost and improve reliability, TI recommends using a 4-mil via at the center pad connected to the ground trace or…
Part Number: TLV7021 Hello
I would like to confirm with you that there is POR time difference of TLV7021 between different temperature.
CH5 is the output of TLV7021. There is a pulse as it is POR of the comparator. The 1st figure shows the POR time…
Part Number: TLV7021 Hello
When I run the TLV7021 simulation. I met some unexpected error.
7021-2023-04-18T09-16.zip
Can you help me solve the problem?
Thanks!
Part Number: TLV7021 Other Parts Discussed in Thread: TLV7011 Hi Team
do you think TLV7021DCKR can replace the NCS2200SQ2TG?
Could it be B2B solution ? or we need tune some RC value.
BRs
Brian
Part Number: TLV7021 Other Parts Discussed in Thread: TLV7041 , TL331B , TLV1861 Tool/software: Hello,
I want to use this comparator (TLV7021/TLV7041) to monitor the input voltage of a device.
However, as the input voltage of the device can be as…
Part Number: TLV7021 Other Parts Discussed in Thread: LMV331-N , LMV331 , TL331 hi team,
Do we have P2P(Same pin layout) alternative for NJU77241F?
Best regards,
Kento