Part Number: TLV7031 I’m building a circuit like the one attached using the TLV7031. In this example, the path from the OUT pin onward is long, so I have currently added a 0.1uF capacitor as a noise countermeasure.
When I run a simulation in this configuration…
Part Number: TLV7031 Hello,
Since I have not worked with low power currents in the uA range before, I would like to ask you before starting the design. I have simulated the circuit below and have a few questions about it.
When I connect R9 at 100kR…
Part Number: TLV7031-Q1 Other Parts Discussed in Thread: TLV1805 , TLV7031 Hi,
The part is used in a +5V circuit with an input range of 200mVpp to 5Vpp. The part is configured for non-inverting hysterisis with a 5k resistor on the +IN and a 1M feedback…
Part Number: TLV7031 I'm designing a circuit for a commercial product and I need some help. I have a 3.3V optoelectronic reflective sensor. When a highly reflective card is placed on the glass the output from the optoelectrical reflective sensor goes…
Part Number: TLV7031 I'm designing a circuit for a commercial product and I need some help. I have a 3.3V optoelectronic reflective sensor. When a highly reflective card is placed on the glass the output from the optoelectrical reflective sensor goes…
Part Number: TLV7031 Tool/software: I'm designing astable multivibrator which generates a clock of 0 to 5V at frequency 800Hz, The circuit is as shown below: Component selection:
Selection of feedback resistor at non inverting terminal
For…
Part Number: TLV7031 Other Parts Discussed in Thread: TLV3231 , TLV9031 Hi Team,
Can you suggest a device that has less delay time but has similar cost compared with TLV7031?
Part Number: TLV7031-Q1 Other Parts Discussed in Thread: TLV7031 Hi Bu team,
Below is a hysteresis comparator designed by a customer. Please review it:
Application Requirements:
When Rntc = 3.735K, Vin1 = 1.08V;
When Rntc=1.66K, Vin2 = 0.72V;…
Part Number: TLV7031 Other Parts Discussed in Thread: TLV1831 Tool/software: Dear Team ,
My circuit and it's output wave-from is given below.
The green color is the output waveform. The amplitude varies from 0 to 2.1V.
This output will be given…
Part Number: TLV7031 Other Parts Discussed in Thread: TLV1851 Tool/software:
VBAT=3V
refer to schematic, when TLV7031 output is static, current comsumption should < 1uA. But current comsumption is about 300uA @output=low; 500uA @output=high And this…