Part Number: TLV7031-Q1 Other Parts Discussed in Thread: TLV1805 , TLV7031 Hi,
The part is used in a +5V circuit with an input range of 200mVpp to 5Vpp. The part is configured for non-inverting hysterisis with a 5k resistor on the +IN and a 1M feedback…
Part Number: TLV7031-Q1 Other Parts Discussed in Thread: TLV7031 Hi Bu team,
Below is a hysteresis comparator designed by a customer. Please review it:
Application Requirements:
When Rntc = 3.735K, Vin1 = 1.08V;
When Rntc=1.66K, Vin2 = 0.72V;…
Part Number: TLV7031-Q1
Tool/software:
Hi expert,
Can TLV7031-Q1 withstand more than 5min X-RAY test? My customer (CosMX) with test all ICs in 5min X-RAY condition. Or do we have X-RAY test standard of TI's devices (including duration, energy, environment…
Part Number: TLV7031-Q1 Tool/software: Hi team,
My customer is using TLV7031-Q1 in their system. They have found one failure mode of VCC short to 16V. The actual measurement is ~10V (because there's resistor in between). Could you please share if the…
Part Number: TLV7031-Q1 Tool/software: Hello. Please help me.
I am currently developing a motor driver board.
The board I am using as a reference for this development uses an IC with the number "C-38AFQLW SNB7031" . However, even after researching…
Part Number: TLV7031-Q1 Other Parts Discussed in Thread: TLV7031 ,
Tool/software:
Hi, Support Team
do we have TLV7031-Q1 for Excel tool to sumulation? could share us? Because our client download TLV7031 PSpics Model but cannot open file of tlv7031…
Part Number: TLV7031-Q1 Tool/software: Hi Ti Team ,
we are using TLV7031QDCKRQ1 as a comparator in push pull mode, we are supply Voltage with resistor divider to Comparator IN- pin but at higher voltages, Lower (-40c)& higher(105c) temperatures observing…
Part Number: TLV7031-Q1 Hi Team,
I'm also having the same issue:
is it allowed if the supply voltage of the TLV7031-Q1 (5V) is turned off and there is still a voltage at the in+ and in- inputs (e.g. 3V) for a long time ?
but the TLV7031-Q1 should…
Part Number: TLV7031-Q1 Hello, Team,
Could you check whether below circuit is OK?:
*コンパレータ = Comparator
Comparator inputs are: - Lo -> Hi @ 2.64V, Hi->Lo @ 1.65V
*Green = Input, Blue: Output
Please note that green is actually a pulse but represented…
Part Number: LM393LV-Q1 Other Parts Discussed in Thread: TLV7032-Q1 , TLV1812-Q1 , , TLV7031-Q1 Tool/software: Hi team,
Our customer is looking for a 5V comparator with similar spec of TLV393LV-Q1, but with push pull output and higher propagation delay…