Thanks for your post James and Clemens for your excellent support.
TLV7041 is probably the best option because of the POR circuit that causes the device to start with high Z output and because the device has integrated hysteresis. This would help keep…
Part Number: LM393B Other Parts Discussed in Thread: LM339 , TLV4021 , TLV7042 , TLV7041 , TLV7021 , TLV7022 , TLV7081 , LM393LV , LM139 Hi,
My customer uses LM393B as voltage detection.
when there is input power and ambient temperature is at >0C, it works normally…
Hi Steve,
you are right, the TLV7041 is open drain and TLV7031 is push-pull. My mistake. But C1 also a problem for an open drain output because a very high short circuit current will flow when the output toggles low. This can cause ground bounce within…
Part Number: TLV3401 Other Parts Discussed in Thread: TLV7041 , The datasheet doesn’t give maximum voltage limit for the open drain output, hence the question in the title.
Thank you!
Part Number: TLV1701 Other Parts Discussed in Thread: TLV7041 Good morning,
Working on a design using the TLV1701 comparator. Looking for the hysteresis characteristics of the TLV1701, VHYS; can't seem to find it in the part data sheet.
With best…
Hello Sean,
I would recommend the TLV7021, or TLV7041 if micropower is desired (they are all on the same datasheet - pick whichever is best for the application).