Part Number: TLV8802 Other Parts Discussed in Thread: OPA2317 , TLV9042 Tool/software: Hi Team,
I'm considering to use TLV8802 as a replacement of OPA2317 as only TLV8802 is registered in customer system. The design is a simple voltage buffer like…
Part Number: TLV8802 Hello! I am planning on using the TLV8802 in a 2-stage amplification circuit, very much like the circuit in the picture below,
I am not very knowledgeable of OP amps. The Unity Gain Bandwidth is 6kHz. Both filter stages (Stage 1…
Part Number: TLV8802 Hi Team,
Customer is looking solution with small package TLV8802 dual OP.
Would you please recommend the proper solution for this?
BR,
SHH
Part Number: TLV522 Other Parts Discussed in Thread: TLV8802 Greetings,
We've have used TLV8802 for a PIR sensor signal amplification circuitry, similar to the one in the TLV8802 datasheet's first page. Would TLV522, which is pin and package compatible…
Part Number: TLV8802 Other Parts Discussed in Thread: OPA2369 , TLV2402 , LPV542 Can the TLV8802 input common mode voltage extend slightly (100 mV) below the low voltage rail? The data sheet limits the VCM from 0 - 4.1V so I suspect the answer is no. But…
Part Number: TLV8802 Other Parts Discussed in Thread: TLV8801 , As I understand the TLV8801 and TLV8802 are the one and two channels variation of the same OPA. But when I look on the supply current characteristics I see that TLV8802 has less curent consumption…
Part Number: TLV8802 Other Parts Discussed in Thread: TLV522 , LPV812 , LPV802 , LPV542 , , OPA2369 , OPA2379 dear Sir
Our IOT project would like to use AD8502ARJZ (SOT23-8) ,May I know TI have Iq=nA 2channel op ??
Thanks
Part Number: TLV8802 Other Parts Discussed in Thread: INA138 , , TINA-TI Hi all,
Since now we are developing a product which need to current sensing of the load (100mA to 7A full range) by 30V supply, then input to MCU A/D for current measurement, before…
Part Number: TLV8802 Other Parts Discussed in Thread: TLV522 , LM324 , LM358 Dear Specislists,
My customer is considering TLV8802 and has questions.
Could you please advise?
---
(1) Generally, optput stage is AB class push-pull.
Can I think TLV8802 is the…