Part Number: TLV6001-Q1 Other Parts Discussed in Thread: TLV9001-Q1 Tool/software: Hi,
My customer wants to use TLV6001-Q1 for high side current sensing.
Current range: 0-20 A
The MCU is a 5V interface.
Please advise on device value selection for 0-20A…
Part Number: TLV9001 Dear Team,
I use the TLV9001IDBVR in a circuit.
Unfortunately there is no availability for this part currently and it has a long lead time.
So I consider TLV316QDBVTQ1 for replacement.
Could you check TLV316QDBVTQ1 can replace TLV…
Part Number: TLV6001-Q1 Other Parts Discussed in Thread: TLV9001 , , TLV9001-Q1 , INA180-Q1 Hi,
The customer experienced a problem with the operation after configuring the circuit.
The circuit increased R101 (Rshunt) from 0.1 ohm to 1.4 ohm, but it does…
Part Number: TLV6001-Q1 Other Parts Discussed in Thread: TLV9001-Q1 , INA180-Q1 Hi,
Customer would like to use TLV6001-Q1 as Diff. Amp as below circuit.
Is each R value correct when using Diff. Amp?
If the value is wrong, please check the recommended value…
Other Parts Discussed in Thread: TLV9001 , TLV9041 , TLV8541 , ADS1114 , TLV9001-Q1 , ADS1113 Hello,
My customer is looking for an OPAMP that can apply non-inverting design under the following conditions.
- Input : Vi = 0V to 100V / 200Hz Sinwave
- Output…
Hello Clemens Ladisch
Thanks for your response.
My understanding is that the LMV3xxA has a similar input structure to the TLV9001, although performance is not guaranteed when the input voltage is near the VCC.
Additional discussion:
For additional discussion…
Part Number: TLV6001-Q1 Other Parts Discussed in Thread: TLV9001 , OPA341 , OPA347 Hi team,
I am Vivek, working as an engineer in Eaton. Here in my application i am using TLV6001QDCKRQ1 to convert differntial input to single ended output. In datasheet it…
Other Parts Discussed in Thread: TS321 , TL074 , TLV9001 , OPA992 , OPA4992 , OPA2992 , LMV831 , OPA345 , LMV821-N , OPA377-Q1 , OPA376-Q1 , OPA377 , OPA376 , TLV376 , TLV9002 The slew rate in my application is slower than the value stated in the data sheet of the op…