Part Number: TLV9024 Hi there,
If I use +5V for the single power supply, and one of the inputs can swing up to the same +5V, will this comparator work normally?
I was wondering if this might saturate the comparator even though VCM range is up to …
Part Number: TLV9024 Other Parts Discussed in Thread: LM339LV I've got a situation where I need an open drain output with a ~2V threshold - TLV9024 seems like a good fit but wanted to check there isn't something newer / better I should be using on this…
Part Number: TLV4H390-SEP Other Parts Discussed in Thread: TLV4H290-SEP , TLV9024 Hello, I'm interested in powering the TLV4H390-SEP with 1.8V(V+) and 0V (V-)
In the data sheet www.ti.com/.../tlv4h390-sep.pdf , the common mode input range is listed…
Part Number: TLV9042 Other Parts Discussed in Thread: TLV9024 Tool/software: Hi Team, My customer has a critical project and we want to promote TLV9042SIRUGR in this project. They need the CAD Footprints (Altium design) which can help to finish the project…
Part Number: LM339 Other Parts Discussed in Thread: TLV9024 Hi Team,
Do we have Pin2Pin device with LM339 but response time less than 0.1us? Thanks.
BRs,
Francis
Part Number: LM339 Other Parts Discussed in Thread: LMV339 , , TLV1702 , LM393B , TLV9024 , LM2903B , TLV7044 Hey!
Are there any comparators similar to the LM339 which come in a QFN package? I did an unfruitful parametric search (likely because I…
Other Parts Discussed in Thread: TLV1704 , TLV9024 , LM339LV Hi Team,
I want to convert the voltage level of multiple logic signals from + 1.8V to - 3.3 V. Is there a level shifter IC that converts to a negative voltage?
If there is no such level…
Part Number: LM339A Other Parts Discussed in Thread: TLV1704 , TLV7044 , TLV9024 , TLV3404 , LM339LV , LM339 Hi TI Experts
LM339APWR VCC:5V ,Positive IN=Reference Voltage=4.5V as below shows.
When the Negative IN rise to about 4.369V then will be…
Part Number: TLV1704-SEP Other Parts Discussed in Thread: LM139 , TLV1704 , LM139-SP , LM139AQML , , TLV7021 , TLV9024 , LM339LV Hello
I was looking for a comparator or operational amplifier to control a NPN base transistor (to be used as a ON/OFF switch…