Part Number: TLV9032 Hi team
,Could you please let us know whether a Functional Safety Manual is available for TLV9032DDFR?
If available, please share the document or provide information on how to obtain it.
Best Regards, Shota
Part Number: TLV9032-Q1 Hello TI-team,
using a TLV903x (push-pull comparator), it says in the absolute maximum ratings, that the voltage on the output should not exceed (V+) + 0.3V. But in the block diagram there are some body diodes of the FETs shown…
Part Number: TLV9032 Hello,
I am using the TLV9032 comperator. In the output i have series diode and resistor of 2 ohm and capacitor to groung of 1uF.
The comperator can handle this load without exceeding the stress?
Thank you
Part Number: TLV9032-Q1 Other Parts Discussed in Thread: TLV9032 , TLV9022 Tool/software: Hi TI,
I have an application in which the inputs of the TLV9032 will see a voltage higher than the supply voltage. Is it OK to clamp the input voltage with the…
Part Number: TLV9032 Other Parts Discussed in Thread: TLV3201 , TLV9022
To give you a brief,
The Aim of the activity is to Add zero crossing detection to the current circuit. The Circuit shown in above figure shows output of a CT connected to Amp…
Part Number: TLV9032 Is an IBIS model available for the output of the TLV9032 comparator? If not, is an IBIS model avaialble for another device that has the same output driver?
Part Number: TLV9032 Hi TI,
Looking at the datasheet (the version found here at least: https://www.ti.com/lit/ds/symlink/tlv9032-q1.pdf ) I noticed that table 6.6 and table 6.8 appear to be identical except for two PSRR entries in table 6.8 which…
Part Number: TLV9032 Other Parts Discussed in Thread: TLV9022 , , TLV3202 Hello,
The Datasheet (Table 6.9) describes the max toggle Frequency (F_TOGGLE) for the TLV9022 (Open Drain version) being ~3MHz (typ) with V_S= 5V. What might the worst case …
Part Number: TLV9032 Other Parts Discussed in Thread: SN74AUC34 , TINA-TI Hello,
Three questions:
Using the SPICE model provided for the TLV9032 online, it looks like the output impedance is not modeled - regardless of the output load it swings…
Part Number: TLV9032 Hi Experts,
There is the spec P ON on page 10 of the datasheet.
There is similar spec T ON in figure 7-1 on page 18.
Are T ON an T ON the same spec?
Regards,
Uchikoshi