Part Number: TLV9034 Hi Team,
Could you clarify if we has only removed the description of the power-on-reset (POR) from the datasheet, or if the entire feature has been removed from the chip? It should be the former, right?
Regards, Hailiang
Part Number: TLV9034 Other Parts Discussed in Thread: TIDA-020069 Subject: TIDA-020069 – Clarification on HVIL Circuit Functional Flow and MCU Interface
Hi TI Team,
We are currently designing a 30 kW DC-DC converter and are planning to implement…
Part Number: TLV9034 Hello!
I am using the TLV9034 and I have a difficulty.
I am using it in the basic mode without hysteresis. The following is a list of characteristics of the schematic:
V+ :3.3V;
V- : 0V(GND);
IN+:input signal,amplitude from…
Part Number: TLV9034 Other Parts Discussed in Thread: LM339 Tool/software: Hello
I would like to design a circuit that detects if a fuse is blown or not in a 600V 60Hz AC system. In the picture below, F1_P and F1_S are two sides of a fuse, and I am…
Part Number: TLV9034 Tool/software: Hi,
I am just wondering what would happen if the inverting input is 5V while the supply voltage is zero. Is it possible for its output to be logic high and will it lead to the other non-inverting input to be high…
Part Number: TLV9034-Q1 Other Parts Discussed in Thread: LM2902B , LM2902B-Q1 , LM2902 , TLV9354 , TLV9364-Q1 , TLV9364 Tool/software: Hi Team,
We were using LM2902B-Q1 before for a current sense op amp. While the slew rate of the LM2902B is slow, then…
Part Number: TLV4H390-SEP Other Parts Discussed in Thread: TLV9034-Q1 , , TLV1704-SEP Tool/software: As stated above we are trying to target 30Krad and at least 30MeV reliability with a pin to pin compatible part. on the same package. We are currently…
Part Number: TLV9034 Hi,
I am using the TLV9034PWR comparator and am facing great difficulty with eliminating chatter at the output. I have followed the datasheet's recommendation for an inverting comparator with hysteresis in section 8.1.2.1, but have…
Part Number: TLV9034-Q1 Other Parts Discussed in Thread: UCC44273 , UCC27517 Hello,
I want to use TLV9034-Q1 to drive 4 different MOS gates.
I want to use full range of output current available for sinking and sourcing (apparently 90-100mA according…