Part Number: TLV9102 Other Parts Discussed in Thread: ADS8862 ,
Dear Technical Support Team,
I have Output Oscillation issue with 2700pF on output.
The configuration is buffer for ADS8862.
When Riso is inserted on output, then output seems to be stable…
Part Number: TLV9102 Hello Sir,
Hope this message finds you well,
I have few questions mentioned below, it will be appreciated if you provide your inputs here.
I am using below Voltage-to-current (V-I) converter circuit with BJT,
https://www.ti.com/lit…
Part Number: LPC662 Other Parts Discussed in Thread: LMC6082 , TLV9102 Hello,
My customer has to redesign the circuit using LPC662 to LMC6082 due to the EOL issued. From the PCN it doesn't get much detail on electrical differences. Has your team done…
Part Number: TLV9102 Hi,
I'm using the TLV9102 for various industrial AIO drivers. These drivers will not be disabled at any time.
Because of this, I want to consistently (and clearly) disable the SHDN (Shutdown) function of the operational amplifier…
HARI T O1 said: Do I need to use a guard trace or can I provide no copper area near the trace as shown below
A guard is needed to stop leakage. The SMA connector should also be connected to guard.
Here is the firs part of a three part article that is very…
Part Number: TLV9102 Other Parts Discussed in Thread: TINA-TI , , TLV9152 , REF3425-EP , OPA2350 , OPA350 , OPA2328 , OPA2613 , LM8272 What is the behavior of this OP if it will be used driving a really large capacitance. I’m thinking about 10 µF (or even larger…
Part Number: TLV9102 Other Parts Discussed in Thread: TLV9152 The TLV9102S is available in the package X2QFN (10).
On the top page of the datasheet in the table “Device Information” the Body Size (nom) of this package is listed as “1.50 mm x 1.50 mm”.…
Part Number: TLV9102 Other Parts Discussed in Thread: PMP10081 , PMP30104 , TLC272 , , TINA-TI Hi support team,
TLC272 is used in PMP10081 and PMP30104.
www.ti.com/.../PMP10081 www.ti.com/.../PMP30104
Is it possible to use TLV9102 instead of TLC272?
Regards…
Part Number: TLV9102 Hello,
Does somebody understand why the Spice model of the opamp TLV9102 takes so long (related to the bias point) to simulate inside Orcad PSpice simulator in comparison with TINA simulator?
Here is the information in title of…