Part Number: TLV9152-Q1 Other Parts Discussed in Thread: TLV9152 Dears,
We have to use VSSOP(8) package dimensions (3mmX3mm) TLV9152QDRQ1/ TLV9002QDRQ1 in our BMS design.
But cad cell for VSSOP(8) package i s not available on datasheet. Can you please…
Hey Cici,
The TLV9154 was suggested as a replacement/upgrade in this design. TLV9154 would not function as a 1 to 1 replacement in simulation to the TLC072, these devices have different characteristics.
TLV9154 is a more up to date part with higher…
Hello,
Just looking at the offset voltages of the amps you mentioned, OPA4990 and OPA4171 already have much lower typical and max offset voltage than LM2902KAV.
OPA4990 has a higher typical offset voltage but a lower max offset voltage over temp range…
Hello,
The circuit shown in the TINA-TI file is not how we recommend measuring the phase margin. I recommend watching our TI Precision Lab Videos on Stability for more information on how to simulate phase margin of a device.
In addition to the method…
Hey Adam,
If you're looking for something that can handle +-12V, and is RRIO, our lowest noise offering is OPAX991. Vn at 1kHz is 10nV/rtHz, and temp range is -40 to 125.
If you just wanted to do single supply 12V and wanted RRIO, OPAX991 is still…
Part Number: TLV9354-Q1 Other Parts Discussed in Thread: TLV9154-Q1 Hi team,
Could you please give me the "Voltage output swing from rail" value over operating temp range of TLV9354-Q1 and TLVx197-Q1
just as specified in TLV915x-Q1 datasheet?
…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…