Part Number: OPA567 Other Parts Discussed in Thread: TLV9161 Hello,
I would like to drive an LED with the OPA567 (up to 500mA). The OPA567 is wired as non-inverted OPA -> 0 ... 3,3V input. Directly at the OPA567 output (PIN 2,3) an POWER-LED is placed…
Other Parts Discussed in Thread: TLV9102 , TLV9101 , TLV9162 , TLV9151 , TLV9161 , TLV9152 Hi team,
do we have device support below request?
device select function;
Channel numbers:1or 2;
VOUT range:0~12V;
VIN range:0~5V;
shutdown current…
Part Number: TLV9151 Other Parts Discussed in Thread: TLV9161 , TLV9051 , OPA323 Tool/software: Hello,
I have a problem with the op amp TL9151SIDBVR. It operates in a differential to single ended circuit. The problem is that for frequencies above 50kHz…
Part Number: LMP7721 Other Parts Discussed in Thread: TLV9161 Hi, team.
I'm designing a trans-impedance amplifier using the LMP7721.
The C2 and IG1 is a model of sensor.
The sensor output is about 0.1~10 nA AC current.
The constant bias of…
Hello Carolina,
See my schematic and the output 60kHz signal.
Right now, I've found interesting discussion concerning very similar issue of the OPA991:
https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/999779/opa991…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…