Part Number: TLV9351-Q1 Other Parts Discussed in Thread: TLV9351 The TLV9351-Q1 is functional safety capable. The TLV9351 is not, right?
What does functional safety capable means exactly for the TLV9351-Q1?
Are there other differences besides the…
Part Number: TLV9351 Dear Sir/Madam,
I am currently calculating the MTBF value for our product, in which we have used the components manufactured by your company.
Therefore, I kindly request you to provide the MTTF and/or FIT value for the below-mentioned…
Part Number: TLV9351 Other Parts Discussed in Thread: TLV9151 , OPA323 , TLV9161 , OPA397 , OPA376 , Hello,
I am closing a design review before committing to a second prototype build, and I have two questions on the TLV9351IDCKR that I cannot resolve…
Part Number: TLV9351 Other Parts Discussed in Thread: OPA196 , OPA182 , XTR111 , XTR105 , XTR117 , XTR116 Tool/software: Hi,
I have designed a circuit to generate a 4–20 mA analog output using PWM. The circuit functions correctly when the output current…
Part Number: TLV9351 When the OPAMP GND shown in red in the design is broken, it pulls from the place shown in blue below and burn the OPAMP. This is a situation we do not want, it is acceptable for the OPAMP not to draw current, but it is unacceptable…
Part Number: TLV9351 Dear e2e team,
I need to supply the TLV9351IDBVR with V+=+3.3V and V-=-5V: looking at the datasheet, at pag 7 table 6.1 there is Vsupply= V+ - V- = 0-42V, instead at table 6.3 is (V+) – (V–) = 4.5 V to 40 V (±2.25 V to ±20 V). …
Part Number: TLV9351 Hello, I am actively using an opamp in the circuit I designed and I want the opamp to turn off its output when the gnd pin is disconnected. However, when the gnd pin is disconnected, the gnd leg of the opamp takes a positive value…
Part Number: TLV9352 I've designed an instrumentation amplifier based on the 3 operational amplifiers topology as the following below. In the design, two op amps are implemented using TLV9352IDR and the third one is implemented with TLV9351QDBVRQ1. Both…
Part Number: TLV9351 Other Parts Discussed in Thread: OPA991 , TLV9151
hi, I have designed a howland current source using tlv9351. From the power rails of the opamp, the gnd pin is externally connected to the connector. When the gnd pin is removed,…
Part Number: TLV9351 Hi sir,
This is Bhuvaneswari from Zettaone Technology,
I need to know few details for the part TLV9351IDBVR
Parts are currently active in the website, may i know how long it will be in production? Is there any EOL issued for…